Because of the holidays, TI E2E™ design support forum responses will be delayed from Dec. 25 through Jan. 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27441EVM-G1A: Difference remaining capacity value

Guru 16770 points
Part Number: BQ27441EVM-G1A
Other Parts Discussed in Thread: BQ24074

Hi

Could you please tell us about behavior of bq27441-G1A.

Companion charger : bq24074
Vin of bq24074 is applied from 5v adapter.

We read Remainingcapacity value by I2C.

Remainingcapacity value which was read after powering on the system (device initialization is done) was different from that of after system load was applied.

And Remainigcapacity value also seems to be depending on whether the adapter is connected or not.
(If adapter is disconnected, remaining capacity decrease less than adapter connecting.)

Is it normal that remaining capacity after system startup is different from that of after system load apply?

If it is normal, is there approach to elimiante difference?

BestRegards

  • Hi Na na78
    It is possible because the gauge runs a remcap simulation at the start of charge or discharge. How much different are they? it shouldn't be starkly different if you configured your gauge correctly.

    thanks
    Onyx
  • Hi

    Thank you for your reply.

    >It is possible because the gauge runs a remcap simulation at the start of charge or discharge.

    Does it mean That a correct remcap value can not be read unless after battery charging or discharging is done once at least?

    >How much different are they?
    For example, 0% is read after initialization but 20% is read after applying load.
    And sometime a correct value can be read even if after initialization.

    I could not understand "configured gauge correctly".
    Should the gauge be configured by I2C after system power up?
    Can you show me detailed procedure? (or document if you have)

    BestRegards
  • No, it means at the start of dsg/chg a simulation is run. Even in relaxation, taking an OCV will also result in remcap sims.

    The gauge should be programmed correctly prior to use by the host. Please use reference documents available on the product page, www.ti.com/.../BQ27441-G1