This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5161: query in Transformer design for Fly buck

Part Number: LM5161
Other Parts Discussed in Thread: ISO5852S,

Hiii,

          I am designing a SIC Mosfet gate driver  &  gate drive power supply.  I have selected ISO5852s  as a driver.  Below are the power supply specifications

Input voltage =  15VDC ( fully regulated)  

switching frequency = 100khz

 two isolated output voltages  

out1 =  +20Vdc ,  50mA   ----   for top Mosfet

out2 =  +20Vdc ,  50mA   ----  for Bottom Mosfet

One non isolated voltage 5Vdc, 100mA   for  primary section of ISO5852s.

since my input dc voltage is fully regulated  &  i decided to go with no feedback from output , which will remove the option of opto-coupler  & also gives the required high isolation from primary to secondary.  

To suit all the above requirements , i decided to use fly-buck topology & selected LM5161.    For transformer  i have selected E25/13/7    N87 material from TDK.  To reduce the core losses & to avoid core saturation at higher temperatures  i decided to limit the Bmax < 200mT.  To limit the Bmax  i need to limit the Magnetic filed strength to ±20 A/m.

I have selected dmax as 33.33% to get 5V ,   which is less than 50% duty. selected turns ratio of transformer as Ns/Np  =  4

From core datasheet Ae=  52.5 mm^2     ,  Le= 57.5mm ,   Al = 1850nH

Np  = ( (15-5) * 3.33)/(0.2 * 52.5) = 3.17  ,  but with 3 turns i am getting only magnetizing inductnace  = 16.65uH .  to increase this i have selected 6 turns , where i am getting = 66.6uH.  Primary peak current =  ( 0.1 + 0.2 + 0.2 + (0.5/2) )  =  0.75A.  

Magnetic filed strength max at this peak current is = ( 6 * 0.75 )/ 57.5  =  78.26 A/m  , which making the transformer to saturate . please check whether the above design calculation is correct or not    &  also suggest me to limit the H value.   Because of the board size limitation i cannot use cores more than E30. Also suggest me if there is any IC from Texas  to  drive forward topology  in open loop .