Other Parts Discussed in Thread: TPS65311-Q1, TPS65251-1, TPS65581
Hi,
I have the following requirements:
Input voltage capable operating at 12V but rated to at least 18V input, operating down as low as possible.
Multiple outputs.
4V @ 2A
3.3V @ 2A
3.3V @ 500mA minimum
5V @ 50mA
1-2.5V @ up to 250mA (super cap charging)
Boost to reuse super cap energy. Ideally I would be able to have multiple taps off of this as well to back up the 4V, 3.3V, and possibly perform a 12V operation.
This last part is the challenge.
Low cost would be a must.
Enable lines for all outputs.
I was able to find the TPS65086 with a quick search but it doesn’t look to have a 4V capability or a boost capability.
Ideally we would want a cap charge circuit instead of basic buck.
Thanks for your help selecting a part.
Feel free to email me offline...
Best Regards,
Blake