This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62173: LiPo Batteries Consistently Burning Hole Above Vin Pin

Part Number: TPS62173

We are using the provided layout in the datasheet, and have verified all of our boards from a benchtop power supply up to 20V input. However, when powering off off 3S (12V) LiPo batteries we are consistently burning holes in the regulator right above the Vin pin. The only load is an LED drawing 5mA. What makes the LiPo input different than the power supply? Is there additional buffering/protection we should add? The datasheet indicates that these regulators are designed for use with LiPo batteries, but that does not seem to be the case. Thanks!