Dear TI expert,
I would like to ask about the mosfet driver in tidu370 which is driving 64x64 pixel LED matrix. There are 32 numbers of Dual P-channel MOSFET being used where they represent 64 lines of the display. I would like to ask if this number can be halved, 16 numbers of Dual P-channel MOSFET only, where a single channel mosfet drive 2 lines of display. I saw that the rated current for the mosfet (APM4953) is 30A, I think this is sufficient because when considering full brightness : 19 mA x 16 channels x 8 ICs = 2.432A. Thank you.
Regards,
Reno