This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2546: Timing interval between EN asserts and USB2 communication

Part Number: TPS2546

Dear Team,

I would like to know is there any timing spec which is relative to EN pin and USB2 communication.

Once EN pin asserts, when will USB host starts to do the USB2 communication with device? 

I think all the steps should be:

Step1: EN pin asserts

Step2: TPS2546 handle BC1.2 protocol to advertise SDP/CDP/DCP

Step3: After BC1.2, USB host starts to communicate with USB device

So do you know the timing between Step1 and Step3? 

Thank you.

Regards,

Jim