Other Parts Discussed in Thread: EMB1428Q,
Hello,
I am currently working with custom 12s active-cell balancing board. Balancing circuitry is made of two identical half-stacks (6s + 6s) based on EMB1428Q + EMB1499Q Chipset. Circuit was made according to TI's Active Chipset Reference Design. Th energy exchange is made between cell and the whole stack.
Both EMB1428Q in design successfully accepts SPI commands and charges-discharges selected cells. However during startup of discharge in lower half-stack a significant ringing occurs in both on both sides of converter: on stack side and on floating side (connected to the cell). The ringing can be seen on the attached graph below:
CH3 (purple) probe connected to PLUS_BOT (positive cell terminal)
CH4 (green) connected to MINUS_BOT (negative cell terminal)
MATH (red) is cell voltage between MINUS_BOT and PLUS_BOT (CH3-CH4)
As it can be seen, first of all negative cell terminal is connected (time at Cursor 1). Then after 156 us positive cell terminal is connected. And when converter turns on huge voltage swing can be seen. As I mentioned before, this behavior is observed when cell is discharged, and only in the bottom side of the stack. And it does not depend on which cell is selected.
Cell current is set to 1 A: Rsense is 0.01 Ohm and Vset is 400mV.
Which part of the circuit can be the source of this problem?
Schematics of the converter and switch matrix are attached below: