This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP55231: lp5523(1) charge pump capacitors

Part Number: LP55231
Other Parts Discussed in Thread: LP5523

Hi,

Is it possible to disable charge pump and omit capacitors connected to C1+ C1-, C2+ C2-  and VOUT and connect VOUT to VDD (5 V) for LP5523(1)? I don't need charge pump as there is 5 V voltage present in my device to supply power for leds.

From datasheet I understood that logic levels are defined by EN voltage. Is that correct? I will interface this driver with 3V3 MCU so EN, SCL, SDA will be 3V3 logic levels.

Are all channels of this driver capable of supplying 25.5 mA simultaneously (if adequate cooling is provided - I guess QFN chip should have no problems with cooling when its pad is connected to ground plane)?