Other Parts Discussed in Thread: PMP8803, TL431, , TPS23751
Hi!
I am read document slva305c, section 2.9-2.10. Equation to calculate Cctl (38) on page 14. How to calculate the Gmo value that is used in this equation?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Tom,
I understood. In expression (38) is error , instead of GMO, |GMO(2*Pi*F0)| should be written.
Thanks!
Hi Tom,
No, I tried to calculate the Cctl value using the value Rctl, Rob and ect. as in the document slva305c.pdf. I did not get the result of 50.3nF.
I decided to do the inverse transform to make sure the original values were correct. In the end, I got that the root expression is negative at the specified values.
Yes, I have problems with re-compensating of my design. Schematic is attached. Input voltage: 36-57V, Output: 24V, 540mA
When design my schematic, I used applications reference designs PMP8803, PMP5595 and document slva305c.pdf.
Thanks,
Sergei
Hi Sergei,
Take a look at the feedback values in the attached 23V reference design (PMP21655). Notice R29: it there to make sure the minimum cathode current is satisfied to allow for regulation (see Imin on TL431 datasheet for sizing that R20 resistor). I recommend adding this.
Also, I recommend significantly reducing your output capacitance. Your output capacitor pole may be too strong. For starters, 22uF may be sufficient.
Keep in mind that PMP21655 uses TPS23751, not TPS23753A & is a type 2 design.
Hello Tom,
I am still working on issue and I have question. What is the capacitor C15 installed for ( PMP21655A(001)_Sch.PDF)?
Thanks,
Sergei