Hello!
I'm searching for suitable circuits/solutions for an AC/DC power supply, 115V/230Vac (85-265Vac) to 24Vdc 25A (600W).
I tried to input these figures in Webench, but there were no suggestions.
A PFC function must be included.
The power supply is intended for the industrial sector and will be produced over a very long period (the previous construction has been produced from the 80s until recently).
Therefore, the components used must be available as long as possible.
It's big advantage if there is reference design(s) availiable.
Does TI has anything to offer?
Thanks!
L-O