Other Parts Discussed in Thread: UCC28951
Customer board occur current spike on current transformer due to the effect of current through.
(Waveform can not attach because of customer confidential)
For example of Typical application(circuit) on the datasheet;
Then the timing of QA gate turn off threshold and QB current turn on by light load condition, current transformer was be spike.
※Light load spec: 140Vout / 1A, spike is around 10A.
Is there recommended process flow to adjust dead time for reduce current spike?
And, is addition to RC filter in front of current transformer good idea?
Best regards,
Satoshi