Other Parts Discussed in Thread: TPS65270
Hello
I would like implement a TPS65270 in one of my new development. For it i took a TPS65270EVM for pretesting.
I made preliminary test on TPS65270EVM in one of certification lab in Israel
The TPS65270EVM should be implement in RF devices, therefore I choose mentioned limits:
EMC (EN 301489-3 Class B) and RF RX mode (EN 300 220-1)
Setup at 3m:
for each output VO1 (5VDC) and VO2 (3.3VDC) I connected 3.3 Ω and 5 Ω in order to get 1 A in each output (not worst case).
Vin 16VDC.
The result:
Green line: EN300 220, RX mode 38.2dbuV/m
Gray: -40/-47 dBuV/m EMC EN55032 Class B
What I made wrong ? how can I fix the exception?