Hi,
I am designing BQ25710 into a charging circuit which uses a 1S lithium smart battery (Level 2), and a USB C PD charging source. The system MCU must be able to communicate with the smart battery at all times when the system is powered, including when VBUS = 0v due to USB source disconnection (when system will be battery powered). The MCU, Battery and BQ25710 share the same SMBus. It is not clear to me what happens tothe SDA / SCL lines of the SMBus interface of BQ25710 when VBUS = 0v, and VSYS is approaching low battery state (<3v).
- Shall the BQ25710 ensure that the SMBus lines are not affected by the low supply voltage and remain high impedance?
- Is the maximum voltage allowed on the SMBus lines affected by VBUS or VSYS voltage?
- Does the BQ25710 remain functioning in low voltage situation? Ie communicable with over SMBus when VBUS = 0v and VSYS = 3v?
- The nominal 6v rail from REGN LDO shall be operating from VSYS rail, but it cannot regulate at 6v. Is REGN and/or VDDA required for operation other than during charging of battery when VBUS shall be present? What is minimum voltage requirement on VSYS when VBUS = 0v?
Thank you,
Tim Warren