This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2695: LM2695

Part Number: LM2695


Dear Sir.

I have some problem with the IC LM2695 , See attached PDF.
The input voltage is 24V ,
Some measurements .
Voltage on pin 9 is  7V , Output Voltage is 0.4V
What should be the voltage at pin 8 .
Please Advise PS.pdfPS.pdf