This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24266: Would you help review our pre-charge data log?

Part Number: BQ24266


Hi 

I had doing data log of BQ24266 charge voltage & current, the pre-charge function seems not meet the charge profile of the datasheet. Would you help review the data log below, if the device are working correctly?

 Riset= 470ohm.

System off mode testing.

Voltage

AvgCurrent

0

0

0

0

0

0

0

0

2907

753

2907

753

2910

654

2910

654

2913

585

2913

585

2917

534

2920

493

2922

459

2924

431

2926

406

2928

386

2930

367

2931

352

2933

337

2934

324

2935

313

2937

301

2937

292

2938

283

2940

275

2940

268

2941

260

2942

254

2943

247

2944

242

2944

236

2945

232

2946

227

2947

218

2947

214

2949

210

2949

207

2950

203

2950

199

2950

197

2952

193

2952

191

2952

187

2953

184

2953

182

2954

179

2954

177

2955

175

2955

173

2955

170

2956

169

2957

167

2957

165

2957

163

2957

161

2958

159

2958

158

2958

156

2959

154

2959

152

2960

150

2960

149

2961

147

2961

146

2961

144

2962

143

2962

142

2962

141

2962

139

2963

139

2963

138

2963

136

2964

135

2964

134

2964

133

2965

132

2965

131

2965

130

2966

129

2966

128

2966

127

2966

126

2967

125

2967

125

2967

124

2967

123

2968

122

2968

121

2968

121

2968

120

2969

119

2969

117

2969

117

2970

117

2970

116

2970

115

2970

115

2970

114

2971

113

2970

113

2971

113

2971

111

2971

111

2971

110

2972

110

2972

109

2972

109

2973

108

2973

108

2973

107

2973

107

2973

106

2974

106

2974

105

2974

104

2975

104

2975

103

2975

103

2975

102

2975

102

2976

101

2976

101

2976

101

2976

100

2976

100

2977

99

2977

99

2977

99

2977

98

2977

98

2978

98

2978

97

2978

97

2978

97

2978

96

2978

96

2979

95

2979

95

2979

95

2979

95

2979

95

2979

94

2979

94

2980

94

2980

93

2980

93

2980

93

2981

93

2981

92

2981

92

2981

91

2981

91

2981

91

2982

91

2982

90

2982

90

2982

90

2983

89

2982

90

2982

89

2983

89

2983

89

2983

89

2983

88

2983

88

2984

88

2984

88

2984

87

2984

87

2984

87

2984

87

2984

87

2985

87

2985

86

2985

86

2985

86

2985

86

2985

85

2986

85

2986

85

2986

85

2986

85

2986

85

2986

85

2986

85

2986

85

2987

85

2987

85

2987

85

2987

85

2987

85

2988

85

2988

85

2988

85

2988

85

2988

81

2988

81

2989

81

2989

81

2989

81

2989

81

2989

81

2989

80

2989

81

2990

81

2990

80

2990

80

2990

80

2990

80

2990

79

2990

79

2990

79

2991

79

2991

79

2991

79

2991

79

2991

78

2991

78

2992

78

2992

78

2992

78

2992

78

2992

77

2992

78

2992

77

2992

77

2993

77

2993

77

2992

77

2993

76

2993

77

2993

76

2994

76

2994

76

2994

76

2994

76

2994

75

2994

76

2994

75

2994

75

2994

75

2994

75

2994

75

2995

75

2995

75

2995

75

2995

75

2995

74

2996

74

2995

74

2996

74

2996

74

2996

74

2996

73

2996

74

2997

73

2997

74

2997

73

2997

73

2997

73

2997

73

2997

73

2997

73

2997

73

2998

73

2998

73

2998

73

2998

72

2998

73

2998

73

2998

72

2998

72

2998

72

2998

72

2999

72

2999

72

2999

72

2999

72

2999

71

2999

72

3000

71

3000

71

3000

71

3000

71

3000

71

3000

71

3000

71

3000

71

3000

71

3000

70

3000

71

3001

70

3001

70

3001

70

3001

70

3001

70

3001

70

3001

70

3002

70

3002

70

3002

70

3002

70

3002

69

3002

69

3002

69

3002

69

3002

69

3003

69

3003

69

3003

69

3003

69

3003

69

3003

69

3003

69

3003

68

3004

69

3003

68

3004

69

3004

68

3004

68

3004

68

3004

68

3004

68

3005

68

3004

68

3005

68

3005

68

3005

68

3005

68

3005

67

3005

68

3005

67

3006

67

3005

67

3006

67

3006

67

3006

67

3006

67

3006

67

3006

67

3007

67

3006

67

3006

67

3007

67

3007

67

3007

67

3007

66

3007

67

3007

67

3007

66

3007

66

3008

66

3008

66

3008

66

3008

66

3008

66

3008

66

3008

66

3008

66

3008

66

3008

66

3009

66

3008

66

3009

66

3009

66

3009

66

3009

66

3009

66

3010

66

3010

66

3010

66

3009

66

3010

66

3010

66

3010

65

3010

66

3010

66

3010

65

3010

65

3010

65

3010

66

3010

65

3010

65

3011

65

3011

65

3011

65

3011

65

3012

65

3011

65

3012

65

3011

65

3011

65

3012

65

3012

64

3012

65

3012

64

3012

65

3013

64

3012

64

3012

65

3012

64

3013

64

3013

625

3155

1841

3167

1836

3171

1833

3174

1830

3177

1827

3181

1824

3183

1822

3186

1820

3189

1817

3194

1811

3196

1809

3198

1809

3201

1807

3203

1805

3205

1804

3207

1802

3210

1802

3212

1799

3214

1797

3218

1793

3220

1793

3222

1792

3224

1793

3226

1790

3228

1792

3230

1791

3232

1791

3233

1786

3237

1786

3239

1786

3240

1785

3242

1786

3244

1786

3246

1785

3248

1785

3249

1786

3251

1785

3253

1785

3254

1785

3256

1785

3258

1784

3261

1784

3262

1783

3264

1784

3266

1783

3267

1784

3269

1782

3270

1781

3271

1780

3273

1782

3275

1782

3276

1781

3279

1779

3281

1779

3282

1778

3283

1780

3285

1779

3286

1778

3287

1778

3289

1779

3291

1779

3291

1778

3294

1778

3295

1778

3297

1777

3298

1776

3299

1775

3301

1775

3302

1772

3303

1774

3305

1775

3307

1775

3308

1775

3309

1775

3310

1775

3311

1774

3313

1775

3315

1775

3316

1775

3318

1775

3318

1775

3320

1775

3321

1775

3322

1775

3323

1775

3325

1774

3326

1775

3328

1775

3329

1775

3330

1775

3331

1775

3333

1775

3334

1774

3335

1774

3337

1774

3338

1774

3339

1774

3340

1774

3341

1773

3342

1774

3344

1774

3345

1774

3346

1774

3347

1775

3348

1771

3349

1763

3350

1765

3350

1765

3351

1767

3354

1767

3355

1768

3355

1767

3357

1767

3357

1768

3358

1768

3359

1767

3360

1767

3361

1767

3362

1768

3364

1768

3365

1768

3366

1768

3367

1767

3368

1763

3368

1764

3369

1764

3371

1764

3371

1765

3372

1765

3374

1764

3375

1763

3376

1764

3377

1764

  • Hi,

    Is your test in customer's system or TI EVM board?

    Could I review your circuit?

    From your setting, it seems CC setting should be 2.55A but from your test, it is only 1.76A, is it correct.

    And from our datasheet, the BAT_short voltage is around 2.9V~3.1V, so just thinking can you also check battery voltage ripple situation? May this case.

    BTW, how about battery voltage is lower than 2.9V condition, is charge current stable?

    Thanks

  • Hi Paul,

    1.  The test done on customer's PCB

    2.  Yes, CC setting is 2.55A .  Current limit is  on type C adapter. (it followed type C adapter current limit)

    3.  The charge current is not stable when the battery voltage is lower than 2.9V.  

    4.  battery voltage ripple waveform and schematics attached below. 

  • Hey PYT,

    The MOSFET Q4 should be a P-Channel FET and it is also currently connected backwards.

    Using a P-Ch MOSFET, the drain should be connected to BAT while the source should be connected to SYS. The forward conduction path of the body diode needs to connect from BAT to SYS.

    Try performing the same test with Q5 removed.


    Regards,
    Joel H