This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM74610-Q1: LM74610-Q1 T0 100%

Part Number: LM74610-Q1

Hi  sir.

     I use the Lm74610-Q1  input 1.5V  and  the load 0.5-0.9A。 It is OK。 But the load in shutdown Mode the load current  is about  20uA 。 the Input has 0.3V Dorp.  It means do not  into T1.