This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Fuel Gauge / State of Charge for 2x NiMH-Batteries

Other Parts Discussed in Thread: BQ34Z100, BQ34110

I am looking for a FuelGauge to measure 2x NiMH batteries in serie (Type: Eneloop).

Our device is powered by these two batteries and the user should know how full the batteries are in about.


The Voltage to measure is 1.6 - 2.8V, capacity of the battery 750mAh, current flow is only about 25mA.

I already tested the BQ34Z100 but it can't measure voltages so low..


Can you please recommend me a chip that would fit for such a simple application?




Best regards and thank you in advance for your feedback,

Joe