Hi,
I have recently powered up a new PCB and have checked the stability of the 5V output.
The design is the same as the Webench simulation. Cin and Cout are made up of MLCC caps.
I expected the output ripple to be around 90mV but actually it is 190mV.
Also the frequency of the ripple is 45kHz but the simulation shows the switching frequency should be around 350kHz.
Would you expect to see the 350kHz frequency at the output?
I can't attach the Webench pdf report to this post but here is the circuit. Also i've attached a scope trace of the 5V output.
Do you have any suggestions I can try to reduce the noise?
Thanks