VFB = Duty x 204 mV; while duty=20%, VFB=20%*204mV=40.8mV;
But from below pic, while duty=20%, VFB=50mV;
I know VREF is from 188~220mV, type voltage is 204mV, but it still has big difference to below pic.
So, I want to know, why both spec are not the same? Which spec I need to refer?