This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61310: the parameter for TPS61310 setting

Part Number: TPS61310
Other Parts Discussed in Thread: LM36010, TPS54201

I want to use this one : TPS61310 , for power supply for mono white LED.

Here is the LED work condition: 3.3V , 1A Forward Current.

I want to load the parameter data to TPS61310 from CPU by I2C, so can you share me the setting data according to the LED infor above?

This is my first time to use this IC, and my project has no time to wait , so I need the setting data by I2C directly.

Thank you very much.