Other Parts Discussed in Thread: TPS62147
I want to know. Switching frequency deviation
· TPS 62140 RGTR
When using 1.25 MHz
Ambient temperature of IC 0 to 70 ° C
VIN 5 to 9.5 V
VOUT = 3.3 V
Average current = about 50 mA
I want to know the swing width to "-" side of 1.25 MHz in particular. It is OK rather than guaranteed value.
vest regards