This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25606: How to using in not connect USB

Guru 11170 points
Part Number: BQ25606


Hello E2E,

I do like to use the bq25606 in USB no connect, will do you have any concern?
Not use D+/D- detection, ILIM is constant (fixed 500mA), Vin is from USB or other 5V.
OTG/CHG mode auto switching by Vin and Vbat detection external circuit.
Are D+/D- is OK left open?

If you have any advice that please let me know.

Regards,