This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CSD17551Q3A: May we know which MOS part more smaller package and also suit use in BQ25703 TIDA-01627 reference design application?

Part Number: CSD17551Q3A
Other Parts Discussed in Thread: BQ25703, CSD87334Q3D, CSD87333Q3D

Hi Sir 

May we know which MOS part more smaller package and  also suit use in BQ25703  TIDA-01627 reference design application?

                                             Bogey

  • Hello Bogey,
    Thanks for your interest in TI MOSFET products. I would recommend the CSD87333Q3D or CSD87334Q3D half bridge power blocks in 3x3 QFN. Both devices are designed for high duty cycle operation and use the same high side and low side FETs. The CSD87333Q3D is rated for 15A continuous current and the CSD87334Q3D is rated for 20A continuous current with lower rds(on) FETs. Can you share the requirements? This will help me determine which power block is best performance/lowest cost for the application.