Other Parts Discussed in Thread: LM5122
Based on the LM5122EVM-2PH development board, I removed the inductors L2 and R21 so that only U1 works. Then replace the output capacitor, Q1, Q2 and loop compensation components C31, R31, C32 and R32, R33, R34. Make the output of the board 48V.
After the test, the board's driving ability is only 1.2A, which can't meet my design requirements. I need 1.5A, so I did the following operation, but I can't increase the output current of the board.
1. Increase L1 and decrease L1
2. Increase output capacitance and reduce output capacitance
3. Increase R2 and decrease R2
What should I do?
I suspect that the drive capability is not enough due to the improper selection of the loop compensation component, but I don't know how to adjust it.
During the debugging process, it was found that the board could start the load normally when it was not connected, and then the load could work normally. However, when the board is started after the load is connected, it cannot be started normally, and the output will be limited to about 32V. What is the reason?