Hi Everyone
Since some size consideration we are planning to split the TIDA-010015 board in two stage like follows
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Everyone
Since some size consideration we are planning to split the TIDA-010015 board in two stage like follows
Hi Salil,
In reference to the above thread for minimizing the form factor , if my power design starting with 120VAC is the maximum input (Ideal case 110V AC to 24DC is our requirement) then accordingly if i design, then the related passive components size get reduced right? do we really need to boost 390V? is there any specific requirement to have 390V DC at PFC output or we can set the PFC boost voltage to some other voltage ?
in that case if my output load is LED load(almost resistive load) then do we really need PFC boost section?
Please advise.
Hi Salil,
"Shielding and decoupling are the important concerns I can think of. High voltage isolation requirements also are required to be met."
High voltage isolation in sense what you are meaning here. Do we need any other isolation technique to be introduced in this power supply? please advise.
Hi Balasubramani,
What I meant was that while splitting the board and stacking them one over the other, it is likely that the high voltage clearance and creepage requirements get impacted. This was a caution to pay attention to see if any potential situation for high voltage isolation violation develops due to the new physical arrangement of components.
Regards,
Salil