Other Parts Discussed in Thread: LMZ31704, , TPSM84A21
Hi,
Using the DC to DC converter LMZ31710 (or might be LMZ31704), I want to control the output voltage by inserting a digital potentiometer as Rset (between VADJ and AGND).
Using the LMZ31710 as the power supply of a Tec device. Input voltage is 12Vdc.
The application is controlling Tec device and so, the target is controilling the Tec temperature output by controlling the LMZ31710 output voltage.
My questions are:
1. Can I do it and in this way to control the output voltage between 0.6V to 5.5V ?
2. If it can be done, do I need to control the Rrt resistor as well? Can I do it with the digital potentiometer as well?
3. If it can be done, what is the setup time of each ouput voltage change? How much time it takes to change output voltage from 0.6V to 5.5V?
4.If it can be done, what is your recommendations for capacitors configuration (input and output), asuming using all the available voltage range (0.6V to 5.5V)?
Thanks in advance,
Amos Daskal