Other Parts Discussed in Thread: TPS65216
What is the purpose of the PB_IN pin on the TPS65217C? We are planning on using the devise with the AM335X Sitara device and the definition of the pin from the TPS65217 data sheet only states:
"Push-button monitor input. This pin is typically connected to a momentary switch to ground. This
pin is an active-low input."
When would the pin need to be momentarily connected to ground in the application with the AM335X and what will temporarily connecting this pin to ground cause to happen?
Thank you.
Stephen Gilbert
Staff Engineer
NORTHROP GRUMMAN
Mission Systems
5000 Bradford Blvd Suite 100
Huntsville, AL 35805
Phone: (256) 327-6772