Other Parts Discussed in Thread: LM5121
We are using the LM5121 on a pluggable board to convert -28V from a chassis backplane to +12V. The +12V feeds two other DC-DC converter to produce +5V and +3.3V. The +12V output is fairly stable when the board is operating in the chassis, but when the board is pulled from the chassis while powered up, the +12V spikes to about +17-20V. This spike is causing catastrophic damage to the downstream DC-DC converters (internal short between +12V input and GND).
The LM5121 circuit was designed by a third party, and they are no longer available to help.
The area that seems to be causing the issue is in the feedback loop. The divider is connected directly between the +12V output and the -28V. So when the board is removed, the -28V jumps toward 0, causing the +12V GND to jump as well, which causes the spike on the downstream DC-DC input and eventually causes the failure. We think that we need something in the RFB2/RFB1 path to stabilize the GND reference for the +12V supply. Not exactly sure the best method for doing that.
Any help would be much appreciated.