Hello,
I'd like to connect the ILM0/1 pins via hardware rather than connecting to a logic device allowing me to change them. I want to use this as a small simple buck supply. I don't see the maximum limits for these two pins in the data sheet? I see the logic high/low thresholds, but I see no value for max voltage on these pins.
1. What are the max voltages I can connect these pins too?
2. Are these generally connected to input voltage or output voltage when hardware strapped?