Part Number: UCC28600EVM
Hello TI Community,
I am trying to accomplish the following: I need a QR flyback controller to take a Vin=48VDC and step it up to an isolated Vout=400VDC at 0.5A output current. I am experimenting with the UCC28600 evaluation board to accomplish this by hacking it apart and modifying it accordingly.
If you recommend a better QR controller than the UCC28600 suited for my application, please advise.
Thus far I modified the following on the EVM board to (try to) suit my needs:
- Replace transformer with another flyback transformer with NS/NP = 3.9 Lm=230uH, soldered OVP resistors directly to the primary winding, and changed both OVP resistor values (R27, R28) accordingly to achieve a desirable voltage at pin 7 (OVP) of the UCC28600 controller. This was successful.
- I am feeding the VDD of the UCC28600 straight from a 9V battery instead of aux. This was successful.
- Replaced secondary side feedback circuit components R36, D16, and C18 with a 9V battery, while adjusting R38, R39, and R40 to achieve Vout = 100VDC at open circuit (for now). Also success.
Right now I am having many problems with trying to attain a 100VDC output (eventually to be 400VDC) to maintain this constant voltage for purely resistive loads ranging from say 200ohms to 1kohm. I have had no success at all in this. I am currently experimenting with different values of R_CS and R_PL, which I understand is also a function of the OVP resistors as well. I am currently trying to use the slvc104j Excel calculator to assist in determining such appropriate values.
PROBLEM: The slvc104j calculator makes numerous assumptions including the use of an AC source, and the use of an AUX winding. What can I do to say "cheat" the calculator to match my situation at hand so that I can attain appropriate values R_CS, R_PL, and R_OVP1 and R_OVP2?
SIDE NOTE: Eventually my converter will be the DC input voltage to an isolated H bridge inverter.
Thank you for your help.