Hi:
I use 5pcs CSD19536KTT MOSFET in parallel on the PCB in my BMS.
I did the battery pack discharging test for the discharging cuurent 50A(32 sec) ---> 80A(15 sec) ----> 100A(5 sec) ---> 200A(5 sec) ----> idle(10 sec) --->50A(32 sec) ---> 80A(15 sec) ----> 100A(5 sec) ---> 200A(5 sec)....
This cycle is always repeat until the battery capacity is exhausted.
Each MOSFET shares the maximum current 40A when the discharging cuurent is up to 200A.
The temeprature of MOSFET is up to 90℃ after the test is done.
After testing several times, I found the 5 MOSFETs of the middle two are occured short and their temperature is over 100℃.
I have no idea of why the reliability of CSD19536KTT is so poor.
Could you have any idea for solving this issue?
Thanks
Morris