Other Parts Discussed in Thread: UCC25600, PMP9750
I'm working on a design with the UCC256304 for 14V 40A output and no PFC. This has the usual split-secondary transformer with two rectifiers feeding a capacitor for the dc output. The handy TI spreadsheet shows a ripple current of 22 amps which seems high and difficult/expensive to manage. Our older product (a hard-switching design but with similar secondary rectifier configuration) has an inductor in series with the rectifiers (which also have RC snubbers) and I found in my spice simulations that this inductor ahead of the output capacitor helps a lot with the capacitor ripple current. However the inductance does seem to reflect back to the primary and affect the resonant drive circuit on the primary side. In my simulation I arbitrarily reduced the primary series inductance to compensate.
My spice circuit is attached, with the two versions compared. Vout1 (green) is output voltage without the output inductor (5V p-p ripple). Vout2 (lt blue) is output voltage with inductor (0.25V p-p ripple). But look at the capacitor ripple - I(C1) (yellow) shows about 80A p-p ripple, while I(c2) (red) shows less than 6A p-p ripple.
The reduction of output capacitor ripple current and output ripple voltage seems to be quite dramatic, although there is some voltage drop.
1. Is this a good approach, and is it advisable?
2. How will this affect the overall efficiency?
3. Should the secondary inductor, as reflected through the transformer, be considered part of the primary inductance?
Thanks!