Dear all
For TPS65094 device, is there any other update replacement materials ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Nick
Thanks your help.
I have a other question:
Question : Is there ready-made special firmware of TPS65094X that can perform below default voltage and timing sequence ? Also, if the kernel voltage can be configured via SVID, it's OK. Please check which device can be suitable.
1. Platform CPU : Intel Apollo Lake N3350/N4200
2. LPDDR4
3. Various voltage:
VCC_VCGI: 0.45-1.3V
VNN_SVID: 0.45-1.3V
VCCIOA: 0.45-1.3V
other voltage
[Image removed - NDA material]
4. Timing sequence
[Images removed - NDA material