Hi all,
We are working on an approximately 400W AC-DC converter using the UCC256301. We are a couple months along, working through some of the details..
One issue we are having is setting the burst mode transition level to a reasonable percentage of the full output power. Right now, even with the top resistor of the LL/SS pin divider removed, the converter stays in burst mode until about 120W (30%).
Maybe someone can confirm if my understanding of the LL/SS pin is accurate. By my understanding, removing the top resistor means no current can flow into the pin, meaning the burst mode threshold (BMT) is at its minimum. With the top resistor added, the LL/SS will sink the current necessary (through the top resistor) to make the voltage on LL/SS equal to VBLK. If the external divider is set so that its output voltage is less than VBLK, then the burst mode threshold will also be at a minimum. This is because, as far as I know, LL/SS can only sink current
Regarding our issue... Typically, the burst mode duty cycle might vary between 1% to 25%, or so. Once it reaches about 25%, the converter flips into continuous operation. On our converter, the burst mode duty cycle continues to increase until it reaches 100% duty cycle (AKA continuous operation).
Any ideas on why this might be the case here?
In addition, in the datasheet, the internal voltage 'AVDD' is referenced heavily but there is no mention of what the value of AVDD, and if its a variable voltage, what drives it. Any input on that?
Thanks a lot!
Tim