Other Parts Discussed in Thread: LM25037
Hello,
My Query is regarding Thermal protection given in section 7.4.6 of the datasheet LM25037/-Q1 Dual-Mode PWM Controller With Alternating Outputs.
The above mentioned section says “Internal Thermal Shutdown circuitry is provided to protect the integrated circuit in the event the maximum rated junction temperature is exceeded.”
- Does the term junction temperature here pertain to the junction temperatures of Power MOSFETS used in Drivers of pin OUTA and OUTB ( Here I'am assuming that Power MOSFETS might be used in Main Output drivers of LM25037 ) ? If it is not then, Can I get some more detailed information regarding junction tempertature of LM25037 IC.
Best Regards,
Shrikrishna