This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61169: output current

Part Number: TPS61169
Other Parts Discussed in Thread: , TPS61500

Team,

Customer is evaluating TPS61169EVM for IP Camera flashing application in below spec requirement.

Vin: single cell battery 3-4.2V

Iout: 200mA

LED#: 4

Based on customer's need, we follow the equation from datasheet and changed R5=1ohm, D1 continuous forward current= 1A, inductor: 10uH or 20uH with Ilrms=2A, but somehow the Iled output current is either lower or higher than expected.

Also in some cases Ilpk seems touched 1.2A minimum current limit threshold though I didn't expect it from estimation. Would you please have a look attached test data and provide some comments or suggest us other solution if tps61169 is not a good one? Thanks.

TPS61169 test data.zip

Thanks.

Allan