Other Parts Discussed in Thread: TPS2491
Hello,
I am using TPS2491EVM-002 with the following changes:
R3 is changed to 47Kohm.
R4 is disconnected.
The following setup was connected:
1. Input power supply 40V 7Amper max limit.
2 A resistor of 7.5 Ohm was connected to the output as a load.
Result:
Current 4 Ampere constant.
Voltage 30 V.
Questions:
1. Why does the current wasn't exceeded to 5Amper according to limit?
2. Why does the FET wasn't turned off the output power?
3. Was there a power limit that cause the voltage to decrease from 40V to 30V? in case the answer is positive please explain how to calculate it s value when R3 is 47Kohm and R4 is disconnected?
Does the expected power limit value shall be : 10 X I lim x 4=> 200Watt
Please explain how to calculate its value?
Regards,
Amir