Hello everybody,
I'm a student and I'm considering an IC drive from TI. I'm building an inverter for my master thesis and I need a specific gatedrive. I'll be using gate driver transformers to secure my drive, but I don't know wich drive is applicable on this concept. For you I added the principle below from the supplier of my gate driver transformers:
www.coilcraft.com/.../gate_drive_transformer.cfm (see figure 2)
Some other specs from my inverter I'm building:
3 phase DC/AC inverter
phase voltage: 400V
switch freq: -16kHz
I max: 8A
In the end I want to make a multi-inverter based on the principle above, but first I want to make it work in single level configuration. Hope you can give me some advice. When you need more information, you can always ask me.
Thanks in advance!