Other Parts Discussed in Thread: TPS62821, TPS54160, LM43603
Hello,
my customer evaluated the TPS57160 using the TPS57160-Q1EVM in which they modified the following: R3, R4 = DNP; R7= 16k; R8=5k2.
Their requirements were the following: Vin = 3.6V, Vout = 3.3V @ 1A. At this input voltage, the device didn't output the expected 3.3V. the value was
Is there a reason for this? is this device suitable for this use case at all?
Regards,
Stani