Part Number: TPS82085
Hello,
I've got a design that uses a TPS82085SIL, and we currently are using a 22 uF AVX 06036D226MAT2A X5R MLCC as the output bulk capacitor. We are looking to possibly swap this part out for a tantalum capacitor, and AVX F380J226MMAAH1.
The data sheet for the TPS recommends a 22uF X7R capacitor, but doesn't mention a recommended ESR limit for the output cap. The tantalum we are looking at has ~0.2 Ohms ESR at 100 kHz, do you know if that added ESR would have an adverse effect on the power supply?
Our input voltage is 4V, output voltage is 1.2V and max current draw for this supply is up to approximately 2 amps. We also have a bunch of MLCCs at the IC we are powering, 1 47uF and then a few 1 uF and 0.1 uF ceramics.
Regards,
David