This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear TI,
I plan to design with the following three solutions.
1. Input : 7V to 24V / Single Output : 15V,0.3A
2. Input : 7V to 24V / Dual Output : 15V,0.15A, 15V, 0.15A
3. Input : 7V to 24V / Tri Output : 15V,0.25A, 15V, 0.1A, 15V, 0.1A
Is there a design problem?
=> When designing with Webench, an error occurs due to input specification problem.
Is there additional tool support for transformer design methods?
=> Webench can only design single output.
Please review and let us have your feedback soon.
If you have any question, please feel free to contact me.
Thank you.