Other Parts Discussed in Thread: BQSTUDIO
Hello,
we are using BQ34z110 for a few years. Now our costumers announced problem with BQ34Z110 in ours device. If they turned off device with full charge Pb battery, when they turn it on the SOC value is jumped down for many percentages. It does not correspond to real consumption.We need repair it at our customers.
At device is used Pb battery 2x7200 mAh (12V) in serial connection.
Ours device has any function states, at each state is different consumption.
States
Turn OFF state S0 - average current 0,6mA (LED is OFF)
The microcontroler in deep sleep mode is periodicly waken up every 2 s for reading data from BQ34Z110 (reading SOC, AI, VOLT, FLAGS) at the state S0 .
S2 average current 61,25 mA (LED flashes (ON 500 ms, 80 mA/OFF 1500 ms, 55 mA)
S3 average current 287 mA (LED is ON)
S4 average current 70,2 mA (LED flashes (ON 500 ms, 82,7 mA/OFF 500 ms, 57,7 mA)
At states S2, S3 and S4 is measuring consumption correct.
We have measured that at state S0 happening jump change of value SOC about 21 % at the one moment. One time we measured at state S0 that SOC value has been 93% for 23 hours 55 minuts and 53 secods after this time SOC value have been changed to 71% although consumption is still the same (0,6 mA). It was happened more times, but we was not able to determine the exact time, it happens any times during weekend (from friday afternoon to monday morning). What could be wrong?
BQ34z110 setting:
[Header]
bq EVSW Version = 0.9.90
DeviceName = bq34z110 v0.04
Time = 1/7/2015 9:48:07 PM
[Safety(Configuration)]
OT Chg = 55.0
OT Chg Time = 2
OT Chg Recovery = 50.0
OT Dsg = 60.0
OT Dsg Time = 2
OT Dsg Recovery = 55.0
[Charge Inhibit Cfg(Configuration)]
Chg Inhibit Temp Low = 0.0
Chg Inhibit Temp High = 45.0
Temp Hys = 5.0
[Charge(Configuration)]
Suspend Low Temp = -5.0
Suspend High Temp = 55.0
Chg Eff = 100
Chg Eff Temp Comp = 25
Chg Eff Drop Off % = 96
Chg Eff Reduction Rate = 10
Maintenance Current = 0
[Charge Termination(Configuration)]
Taper Current = 100
Min Taper Capacity = 25
Cell Taper Voltage = 100
Current Taper Window = 40
TCA Set % = 99
TCA Clear % = 95
FC Set % = 100
FC Clear % = 98
DODatEOC Delta T = 10.0
[Data(Configuration)]
Rem Cap Alarm = 100
Design Cell Voltage = 2000
Initial Standby = -10
Initial MaxLoad = -500
Manuf Date = 01-Jan-1980
Ser. Num. = 0001
Cycle Count = 00
CC Threshold = 900
Design Cell Capacity = 7350
Design Cell Energy = 14700
SOH Load I = -400
TDD SOH Percent = 90
Cell Charge Voltage T1-T2 = 2250
Cell Charge Voltage T2-T3 = 2450
Cell Charge Voltage T3-T4 = 2350
Charge Current T1-T2 = 10
Charge Current T2-T3 = 50
Charge Current T3-T4 = 30
JEITA T1 = 0
JEITA T2 = 10
JEITA T3 = 45
JEITA T4 = 55
ISD Current = 10
ISD I Filter = 127
Min ISD Time = 7
Design Energy Scale = 1
Device Name = bq34z110
Manufacturer Name = Texas Inst.
Device Chemistry = PbA
[Discharge(Configuration)]
SOC1 Set Threshold = 150
SOC1 Clear Threshold = 175
SOCF Set Threshold = 75
SOCF Clear Threshold = 100
Cell BL Set Volt Threshold = 1800
Cell BL Set Volt Time = 2
Cell BL Clear Volt Threshold = 1850
Cell BH Set Volt Threshold = 2450
Cell BH Volt Time = 2
Cell BH Clear Volt Threshold = 2400
[Manufacturer Data(Configuration)]
Pack Lot Code = 0000
PCB Lot Code = 0000
Firmware Version = 0000
Hardware Revision = 0000
Cell Revision = 0000
DF Config Version = 0000
[Integrity Data(Configuration)]
Static Chem DF Checksum = 7CD5
[Lifetime Data(Configuration)]
Lifetime Max Temp = 30.0
Lifetime Min Temp = 14.9
Lifetime Max Chg Current = 1425
Lifetime Max Dsg Current = -798
Lifetime Max Pack Voltage = 29964
Lifetime Min Pack Voltage = 6024
[Lifetime Temp Samples(Configuration)]
LT Flash Cnt = 138
[Registers(Configuration)]
Pack Configuration = 0960
Pack Configuration B = FF
Pack Configuration C = 30
LED_Comm Configuration = 00
Alert Configuration = 0000
Number of series cell = 12
[Lifetime Resolution(Configuration)]
LT Temp Res = 1.0
LT Cur Res = 100
LT V Res = 25
LT Update Time = 60
[LED Display(Configuration)]
LED Hold Time = 4
[Power(Configuration)]
Flash Update OK Cell Volt = 1000
Sleep Current = 10
FS Wait = 0
[Manufacturer Info(System Data)]
Block A 0 = 00
Block A 1 = 00
Block A 2 = 00
Block A 3 = 00
Block A 4 = 00
Block A 5 = 00
Block A 6 = 00
Block A 7 = 00
Block A 8 = 00
Block A 9 = 00
Block A 10 = 00
Block A 11 = 00
Block A 12 = 00
Block A 13 = 00
Block A 14 = 00
Block A 15 = 00
Block A 16 = 00
Block A 17 = 00
Block A 18 = 00
Block A 19 = 00
Block A 20 = 00
Block A 21 = 00
Block A 22 = 00
Block A 23 = 00
Block A 24 = 00
Block A 25 = 00
Block A 26 = 00
Block A 27 = 00
Block A 28 = 00
Block A 29 = 00
Block A 30 = 00
Block A 31 = 00
[IT Cfg(Gas Gauging)]
Load Select = 2
Load Mode = 1
Max Res Factor = 15
Min Res Factor = 3
Ra Filter = 500
Fast Qmax Start DOD % = 92
Fast Qmax End DOD % = 96
Fast Qmax Start Volt Delta = 100
Cell Terminate Voltage = 1800
Cell Term V Delta = 25
ResRelax Time = 200
User Rate-mA = 0
User Rate-Pwr = 0
Reserve Cap-mAh = 0
Reserve Energy = 0
Max Scale Back Grid = 4
Cell Max DeltaV = 100
Cell Min DeltaV = 0
Max Sim Rate = 2
Min Sim Rate = 20
Ra Max Delta = 44
Qmax Max Delta % = 5
Cell DeltaV Max Delta = 10
Fast Scale Start SOC = 10
Charge Hys V Shift = 40
[Current Thresholds(Gas Gauging)]
Dsg Current Threshold = 60
Chg Current Threshold = 75
Quit Current = 20
Dsg Relax Time = 60
Chg Relax Time = 60
Quit Relax Time = 1
Cell Max IR Correct = 400
[State(Gas Gauging)]
Qmax Cell 0 = 7344
Cycle Count = 0
Update Status = 02
Cell V at Chg Term = 2466
Avg I Last Run = -712
Avg P Last Run = -1413
Cell Delta Voltage = 1
T Rise = 20
T Time Constant = 1000
[OCVa Table(OCV Table)]
Chem ID = 0804
[R_a0(Ra Table)]
Cell0 R_a flag = 0000
Cell0 R_a 0 = 45
Cell0 R_a 1 = 39
Cell0 R_a 2 = 32
Cell0 R_a 3 = 29
Cell0 R_a 4 = 25
Cell0 R_a 5 = 23
Cell0 R_a 6 = 20
Cell0 R_a 7 = 21
Cell0 R_a 8 = 21
Cell0 R_a 9 = 22
Cell0 R_a 10 = 23
Cell0 R_a 11 = 23
Cell0 R_a 12 = 23
Cell0 R_a 13 = 23
Cell0 R_a 14 = 23
[R_a0x(Ra Table)]
xCell0 R_a flag = 0055
xCell0 R_a 0 = 45
xCell0 R_a 1 = 39
xCell0 R_a 2 = 32
xCell0 R_a 3 = 29
xCell0 R_a 4 = 25
xCell0 R_a 5 = 23
xCell0 R_a 6 = 20
xCell0 R_a 7 = 21
xCell0 R_a 8 = 21
xCell0 R_a 9 = 22
xCell0 R_a 10 = 23
xCell0 R_a 11 = 23
xCell0 R_a 12 = 23
xCell0 R_a 13 = 23
xCell0 R_a 14 = 23
[Data(Calibration)]
CC Gain = 10.357
CC Delta = 10.337
CC Offset = -0.67
Board Offset = -0.21
Int Temp Offset = 0.0
Ext Temp Offset = -.9
Voltage Divider = 37586
[Current(Calibration)]
Deadband = 5
[Codes(Security)]
...
Thanks you for your help.
Best regards
Tomas Samek