Dear team,
we understand the EN pin must not be tied to VIN as it is limited to 6.5V. We also understand I can be left floating to turn on because the is internal 300nA current source pulling up the signal. This is then clamped by an internal 6.5V Zener. This lead to the assumption that the Zener can digest a certain continuous current during normal operation.
Because of second source qualification the layout and population of the board needs to be done such, that another LDO can be installed which needs to have the EN connect to VIN. We can not ensure the resistor is NOT populated in case of TPS709.
So here is the questing. We hope that a high ohmic resistor still can be connected from EN to Vin. The question would be how much current can we allow into the internal clamping 6,5V Zener in addition to the 300nA. Is this feasible at all and what resistor value can we use for Vin = 15V?
many thanks
Lutz