This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27621-G1: BQ27621YZFT-G1A

Part Number: BQ27621-G1

hi,

we are seeing a high number of BQ27621YZFT-G1A devices that appear to be failing in the same way.

on the units that fail vdd and vss measure 3-5ohms whereas a unit that works measures 35ohms plus.(device fitted to board)

if the chip is removed the 3-5ohms can be measured between the vdd and vss pins on the device itself.

on the units that fail the unit will power up with a battery connected but there is no vdd output.

I have tried toggling a vdd voltage as suggested on another post but it made no difference.

the boards are assembled in an antistaic environment so I do not believe that it is an esd problem.(which another post suggested can lock up devices).

is it possible that the devices are shipped from the manufacturer with different "states" of the vdd output?

if so is there a command that needs to be issued to remove the device from that state which is giving the low impedance output?

any help or suggestions would be appreciated