Other Parts Discussed in Thread: BOOST-PSEMTHR-007, TPS23880EVM-008, TPS23880
Hi All,
I'm testing the TPS2372-4EVM-006 evaluation module against several switches and injectors that we have in site. The TPS2372-4EVM-006 has been configured as Class 6 ( 51w at the PD). Every time I connect BT PD Class 6 to an AT PSE device it shows TPH = High, TPL = Low , BT = High, which I agree as it's a demotion case using an AT PSE.
There has been a case where an AT injector didn't turn on the BT PD Class 6. I had to set the BT PD as Class 4 and then it was capable to turn the PD on and it was able to supply the full power needed by the application ( it is a 60w injector). I guess the reason is because it is an POH PSE, but it is not specified in the injector datasheet ( or at least that is what I think). I guess this suggests that I need to set the capability to the end user to switch between Class 4 and Class 6 as POH won't turn on if the PD is set to Class 6. I guess I'm not the first one on this situation, I'm thinking to use a switch to change between Class 6 and Class 4, but I guess there will be more solutions, any idea?.
Is it common for POH PSE not to specify that they are POH?. Before the development of BT PDs and BT PSEs I can't find a reason to distinguish between AT PSEs and POH PSEs, is there any?.
If I give you the part number of the injector that I have mentioned could you confirm that it is a POH injector?.
Thanks in advance,
Daniel.