Other Parts Discussed in Thread: CC3220SF, , EV2400, BQSTUDIO, GPCCEDV
Hello I am working on a project that has the BQ34110 and I want to read information off some NiMH D-Cell rechargeable batteries. I am using a CC3220SF launch pad. Basically the batteries need to power the launchpad for over 30 days and I need the BQ34110 to output the battery voltage and current to know when to replace the batteries.
My question is how do I connect these two together and how to interface between the two? I know I need I2C so can you point me to an example on how to use I2C with the CC3220SF and BQ34110.
I have read the "Using I2C communications with bq34110" report but I am not sure how to program the bq34110 using CCS and CC3220SF.
Any help is greatly appreciated. Thanks