Hello E2E,
From reading section 8.4 in the datasheet and had some remaining questions about the LDSTRT. Mainly this section:
"Except the LDSTRT fault, all the other faults can also be reset by an internal auto-retry logic which can be either disabled or configured by user to perform a limited or infinite number of retries with a programmable delay between retries. The auto-retry behaviour is controlled by the connections on the RETRY_DLY and NRETRY pins."
We would like to use it as a way to force a reboot of the system, but the excerpt makes me think we can't do that. It sounds like once a LDSTRT fault is triggered we have to cycle main power or the enable pin somehow. Is that accurate?
Thanks!
Russell