This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS22990: TPS22990: Is there a maximum CT(pF)/output rise time spec?

Part Number: TPS22990

My setup :

TPS22990

VIN 5V

VBIAS 5V

ON connected to VIN 5V

Ct of 0.47 uF

CIN 1.0 uF

COUT 0.1 uF

Cload ~ 300 uF

T rise is measured at 1 ms, I expect at least 15 ms. Is the switch capable of 15 ms T rise under these voltage and load conditions ?

Thanks