This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61021A: about Vref accorfing to input.

Part Number: TPS61021A


My customer have some problem with TPS61021A.

Their spec is input 0.9V~2.7V.

Output is 4V@0.5A.

No load 

When input  is 0.9 V, Vref is 240mV  and output voltage is 1.0V

When input  is 1.1 V, Vref is 360mV  and output voltage is 1.6V

When input  is 1.3 V, Vref is 440mV  and output voltage is 1.8V.

When input  is 1.5 V, Vref is 560mV  and output voltage is 3.2V.

When input  is 1.8 V, Vref is 800mV~900mV  and output voltage is 4.1V~4.2V

under 1.8V, Vref is unstable and out voltage is untable.

How do I fix this issue?