I plan to charge the battery of my IoT device with the BQ24210.
The charger will be permanently connected to the Li Ion battery (18650 1cell, 3200 mAh)
Solar panel will be : Voc = 6V, Vmp = 4.4V, Imp = 500-750mAh
EN tied to PG (no LOAD mode)
Riset 780 Ohm
Rchg=Rpg=2K Ohm
Vdpm will float , unconnected
I wonder, in order to extend the life of the battery, is it possible, after the completion of the charging, to set up some how IC to wait for the battery voltage to decrease lets say to 3.5V in order to reactivate the recharge process again ?